Why You Should Not Intermix Tube Fittings
Why You Should Not Intermix Tube Fittings From Different Manufacturers
Fluid and analytical instrumentation systems rely on dozens of quality components working harmoniously to keep operations running efficiently. Any performance lapses can result in leaks, potential safety concerns, and system downtime.
One way to prevent these issues is to build your fluid systems with tube fittings from a single manufacturer. Claims that tube fitting components can be intermixed and interchanged with those of different manufacturers should be questioned — intermixing and interchanging can be risky and may compromise worker safety. And no one wants to introduce unnecessary risk into their system’s operation.
Do you or your installers regularly intermix or interchange tube fittings? Let’s explore the reasons why tube fitting intermix and tube fitting interchange can lead to poor fluid system performance:
What Is Tube Fitting Intermix and Interchange?
First, it is important to understand the differences between intermix and interchange:
An intermixed or interchanged fitting is essentially a new, untested design.
Some manufacturers may claim that their products are interchangeable with other brands. Manufacturers making these claims typically say that doing so can help save an operator on costs.
But no manufacturer can reliably and uniformly replicate designs from that of a competitor, and any resulting failure will certainly void any short-term savings. Tube fitting components from different manufacturers are not explicitly designed to work together. Thus, an intermixed or interchanged fitting is essentially a new, untested design. Interchanged and intermixed fittings may demonstrate:
- Inconsistent sealing surfaces due to design, construction, and torque value differences
- Sealing surface incompatibilities due to geometry, tolerances, and metallurgic properties
- Compromised function
- Fatigue failure
- Ineffective sealing surfaces resulting from different swaging mechanisms, material hardness, and tolerance variations
For these reasons, interchanging and intermixing tube fitting components can lead to unpredictable performance, increased costs, and potential safety hazards. Intermix and interchange may also void your warranty. For example, intermix and interchange will void Swagelok’s Limited Lifetime Warranty, which can lead to even higher costs if and when a problem occurs.
Always Avoid Tube Fitting Intermix and Interchange
Avoiding intermix and interchange is a best practice promoted by numerous fluid systems standards agencies. For example, the IOGP JIP-33, an initiative aimed at making dramatic improvements in the specification, procurement and delivery of oil and gas equipment, specifically calls tube fitting intermix and interchange a “bad engineering practice.” Single-sourcing your tube fittings from one reliable supplier is a good way to avoid potential interchange and intermix, even by accident. When only one brand is available, technicians cannot mistakenly combine components from two different manufacturers.

You May Also Like
These Related Stories

Fitting Training: How to Install Tube Fittings

How to Detect and Prevent Fluid System Leaks