Swagelok tubing and accessories
Find reliable tubing options with the material properties needed for your application. Ensure your system is built to last with tubing accessories that help you cut, bend, deburr and support tubing to ensure leak-tight performance.
Download tubing documentation
Get information in one email, including manual and catalog on manual tube benders and catalogs on stainless steel seamless tubes, sheathed tubes, insulated bundles and more.
Selection of tubing & bending services
The unsurpassed quality of Swagelok tubing derives from extraordinarily high quality materials, thoughtful design, and manufacturing controls. Pair that with our local services like tube bending, training seminars, and selection support, and you get even more value.
Selection and support
Swagelok simplifies material selection for various systems, leveraging decades of expertise in combating corrosion since 1947. Their alloys, with optimized multi-element compositions, offer superior corrosion resistance, enhancing product performance.
Tubing bending
We can bend tubing to size for you in our own workshop. Many sizes, materials and wall thicknesses are possible.
Pre-fabricated assemblies
You know using bent tubing instead of traditional piping in some common applications can slash potential leak points and installation time. Now save even more with fully built, leak-tight assemblies that incorporate your pre-bent tubing.
Certificates
Expertise
Stock
Production
Reliability
Training
Swagelok tubing for any industrial application
With 200 active patents, Swagelok supports the most critical applications and industries. You can find our tubing in tens of thousands of industrial plants worldwide. Here are some of your options:
Our local team offers quick quotes, product selection advice, and daily shipping. If we can help in any way, please message us.
Material selection guide
Learn about types of corrosion, materials most commonly affected, and designed combinations you can rely on. Read the page or email the brochure.
Saving with fully built assemblies
We design, manufacture and test fluid system assemblies for customers, here in Waddinxveen
Tube bending techniques
Gaining experience and knowledge in the theory and practice of tube bending is essential. By learning the measure-bend method through practical assignments, one can master an efficient bending technique.
Videos
Download "hidden costs of leaks" guide
Download this excerpt from the Tube Fitter's guide to learn the Leak Formula and best practice examples for prevention.
Frequently asked questions
When selecting a type and size of tubing for a job, we recommend you consider:
- Surface finish
- Material
- Hardness
- Wall thickness
With just those four factors you can come up with thousands of permutations. To help you narrow down your choices, Swagelok has developed tubing data sheets. There are separate sheets for more than a dozen different materials such as carbon steel, copper, aluminum and a variety of alloys.
Watch out for bends. When installing fittings near bends in the tubing, you need to make sure that you leave enough straight length in the tubing to properly bottom the tubing out in the fitting. How much is enough? The tubing data sheet provides a handy chart to help you.
To get our tubing data sheet, see the "Download Tubing Documentation" option at the top of this page.
Tapered pipe threads are one of the most common end connections in the industry. They are relatively easy to make, but they always need a sealing compound because there are designed gaps between the male and female wires.
This video covers preparation, tape size, winding procedures and subsequent tightening.
Indeed, the quality of tubing can vary greatly between different manufacturers. Here are some important points to look out for before installing tubing in a Swagelok fitting:
- Seamless or welded: Check whether the tubing is seamless or welded.
- Hardness: What is the hardness of the tubing?
- Surface finish: Make sure the surface is free of scratches.
- Ovality: Check the ovality of the tubing.
- OD and ID: Check the outer diameter (OD) and inner diameter (ID) to make sure they are free of burrs.
- Wall thickness: Make sure the wall thickness is adequate for the pressure the system will see.
- Concentricity: Check that the wall thickness is the same throughout.
The pressure rating of a Swagelok tube fitting depends on the lowest rated component in the system in which it is installed. Sometimes the lowest pressure rated component is a pipe thread, a pressure gauge, or a valve. Other times it will be the pressure rating of the tubing itself, and that will vary depending on the tubing's size, wall thickness and material of construction.
In general, it is best to use the same materials. There are exceptions.
Example: if you have stainless steel pipes, use stainless steel ferrules and fittings. For plastic pipes, use plastic ferrules and fittings. The reason for matching materials is simple: you want the ferrules to be stronger than the pipes, so the ferrules can clamp onto the pipes and stay in place. This video explains more:
If the ferrules are made of a softer material than the tube, you won't get that clamping effect. Brass, for example, is softer than stainless steel. So brass ferrules will not give full clamping action on stainless steel pipes
When properly installed, Swagelok fittings produce a repeatable, leak-tight seal even after being reassembled multiple times. Before disassembly, mark a line along the nut and body flat and use these marks to ensure that the fitting is reinstalled properly. Please watch the video demonstration below for the proper instructions:
If you have made changes in the system design, by moving a fitting to a new location or changing the tubing, you can't re-use the nuts and ferrules, but you can still re-use the fitting bodies. Even on a simple connector, you are saving a big percentage of the cost of using all-new parts. Think of a cross or a tee that is more robust - there is a huge cost savings opportunity there.
For personalized, up-to-the-minute answers to sales and support questions, please use green buttons on this page to request details/quote.
If you prefer to find answers yourself, visit products.swagelok.com, register for an account, and start exploring. Anyone can register, and completing the entire registration form will allow you to view pricing, order online, request quotes, store favorite products, assign customized part numbers, and save or forward your shopping cart.