Always in control of your gas distribution system

Certainty about security, performance, and audits.
No leaks, downtime, or stress.

Schedule a consultation Email to me

Gas distribution is extremely important for your business processes. But risks often creep in unnoticed: outdated installations, leaks, or inefficiency. Swagelok helps you make your system smarter, safer, and future-proof.

Why examine your system?

Without you knowing it, invisible risks can arise. Consider, for example:

 

Does this sound familiar? Then it's time for a check-up.

Schedule a consultation

Gas distribution systems without downtime

Swagelok speaks the language of technology and compliance.

As an engineer, QA manager, or facility manager, you bear the responsibility. With over 75 years of experience in gas and fluid systems and specialist knowledge in systems within industries such as Oil & Gas, Chemicals, and Education, Swagelok is a strong partner you can rely on and trust. While our components are recognized worldwide, our assistance, support, and audits are locally oriented. Close by and committed.

Design Gasdsitribution systems

Five steps to a secure and reliable system

1. Initial consultation

Together, we take stock of everything from the situation and risks to specific wishes..

2. Survey

By thoroughly analyzing your current system, we gather valuable insights.

3. Advice

You will receive a professional yet practical report with tailored recommendations.

4. Design & assembly

Efficient, secure, and future-proof. Where are the opportunities for optimization, and how can we implement them in existing processes and systems?

5. Aftercare

Our service does not end after installation. We offer ongoing support for maintenance or expansion.

Schedule a consultation

What are the ultimate benefits for you?

✓ Less downtime and malfunctions
✓ Leak-proof system with reliable performance
✓ Greater control over processes and documentation
✓ Peace of mind and control during audits and inspections
✓ Lower costs due to preventive maintenance

Work we and our customers are proud of

After standardization with Swagelok panels:

  • $52,000 savings on replacement every 5 years
  • 75% less maintenance time
  • Reduced emissions by eliminating leaks
  • Better audit preparation

At a leading chemical company, Swagelok identified opportunities to standardize the design of gas panels.

Swagelok’s gas distribution systems help us reduce both operational costs and gas consumption

Chemical company England

Frequently asked questions from our customers

When does my system need to be replaced?

Replacement is recommended in case of structural leaks, worn connections, changed process requirements, outdated standards, or when audits reveal deficiencies.

What makes Swagelok different?

Customized solutions, high-quality components, local support, and proven reliability.

How quickly can an analysis start?

Within a few days after intake. Duration depends on your current system.

How often should a gas distribution system be inspected?

In industrial environments, annual inspections are recommended. In laboratories, inspections may vary from semi-annual to annual, depending on the type of gas and the criticality of the processes.

What materials are used in gas distribution systems?

Common materials include stainless steel, copper and special alloys. The choice depends on the type of gas, purity requirements, and pressure conditions.

Do you provide support with design and installation?

Yes, we support the full process: engineering, design, material advice, assembly, testing, documentation, and installation guidance. Ask us for a consultation and see how Swagelok can help.

Contact us

Want to know more about our gas distribution modules?

Swagelok Source Inlet (SSI)

Swagelok Source Inlet (SSI)

  • Safe replacement of gas cylinders with purge and venting options.
  • Connection between source and distribution system.

The source inlet connects the high-pressure gas source and the distribution system. It is important that the inlet is built with appropriate cylinder connections, hoses, tubing, filters and venting, flushing and relief functions to ensure that gas can be safely fed to the primary gas pressure control or automatic changeover. For a single gas cylinder, the assembly may be as simple as a hose and connector. Multiple cylinders may require a manifold with many hoses and valves.

Swagelok Gas Panel (SGP)

Swagelok Gas Panel (SGP)

  • Initial pressure reduction of source gas.
  • Modular design, easy to maintain.

As the primary gas pressure control, the SGP completes the initial pressure drop of the source gas and ensures it is delivered to the next stage of the system at the proper flow rate. Pressure reduction is achieved in one stage with a single pressure regulator or in two stages through a dual pressure regulator arrangement.

Swagelok Changeover (SCO)

Swagelok Changeover (SCO)

  • Automatic switching between sources.
  • Continuity and less waste.

The automatic changeover system switches seamlessly from one gas source to another to ensure an uninterrupted supply. This is achieved through staggered set points of two pressure regulators, allowing the system to continue operating while the primary gas source is changed. Our switching station allows for customized switching set points to reduce wasted gas in cylinders.

Swagelok Point of Use (SPU)

Swagelok Point of Use (SPU)

  • Local pressure control for workstations or equipment.
  • Compact, accurate, standardizable.

The point-of-use system provides the critical final stage of pressure control before gas is used. These are often the least complex of the four main systems, usually involving a pressure regulator, pressure gauge and shut-off valve. Usage point systems offer operators and technicians a convenient and accurate method of adjusting pressure to suit their test bench or equipment needs.

Read detailed information about gas distribution systems

Swagelok offers more than gas distribution systems


Schedule a consultation

TechTalk Gas Distribution

A half-hour technical presentation. In this video, an expert shares his knowledge on a specific topic, with numerous practical examples, applications, and advice.

Ready for a safer and more efficient gas distribution system?

Featured articles

Understanding modern gas distribution systems: part 4
Safety and efficiency in modern gas distribution systems

Understanding modern gas distribution systems: part 4

Understanding modern gas distribution systems: part 3
Safety and efficiency in modern gas distribution systems

Understanding modern gas distribution systems: part 3

Understanding modern gas distribution systems: part 2
Safety and efficiency in modern gas distribution systems

Understanding modern gas distribution systems: part 2

Read More

Read additional pages on Gas Distribution Systems below