Swagelok fittings
Fittings are an important component in fluid systems, providing the essential connections from one component or section to another in various applications. Fittings must be reliable because leaks from fittings can result in lost production and additional labor hours required to make repairs or replacements. If there is leakage then it affects industrial, human and environmental safety.
Download Swagelok fitting documentation.
In one click you will receive a Digital Catalog, aTubing Data Sheet, theInstaller's Pocket Guide and other informational materials.
The value of a Swagelok tube fitting
Swagelok fittings, also known as twin-ferrule fittings, give reliable performance, provide less maintenance, reduce safety hazards and/or unintended emissions. When properly installed, they provide a leak-free connection year after year, even after being reassembled several times.
Fittings with twin-ferrule construction provide:
- tube grip
- gas seal
- vibration resistance
They are easy to install and can be used repeatedly, even after de-assembly. For more than 75 years, the safety and reliability of Swagelok fittings has been proven.
Stronger tube grip
The hinging collecting action in a Swagelok tube fitting puts more of the back ferrule's surface in contact with the tubing. That means more material for direct axial support and colleting squeeze. You don't get that with a bowing ferrule or with the bite type of ferrule.
Stronger gas seal
A Swagelok tube fitting forms a gas seal by means of the burnishing that occurs in two places: between the front ferrule and the tube fitting body, and between the front ferrule and the tubing. With Swagelok, you get a stronger seal under maximum working pressure.
Stronger vibration protection
The patented case-hardening process and back-ferrule geometry provide excellent vibration fatigue resistance and tube support—even in harsh or stressful environments, such as hydrocarbon processing, on-vehicle applications, or rotary equipment applications.
Certificates
Expertise
Warranty
Installation
Material
Reliability
Reuse
Safety
Training
A Swagelok fitting for every industrial application
Our founder invented the two-ferrule tube fitting in 1947. With 200 active patents, Swagelok supports the most critical applications and industries. You can find our fittings on the surface of Mars, at extreme depths in oceans, and in tens of thousands of industrial plants worldwide.
Our local team offers quick quotes, product selection advice, and daily shipping. If we can help in any way, please message us.
Download material selection guide
Learn about types of corrosion, materials most commonly affected, and designed combinations you can rely on
Videos
Tube fitting installation training
Comprehensive training on the operation, assembly and use of Swagelok fittings.
Download "hidden costs of leaks" guide
Download this excerpt from the Tube Fitter's guide to learn the Leak Formula and best practice examples for prevention.
Are .... and Swagelok fittings interchangeable??
Do not mix or interchange product components with those of other manufacturers. Doing so voids the Swagelok warranty.
Fluid and analytical instrumentation systems rely on dozens of quality components working harmoniously to keep operations running efficiently. Any performance lapses can result in leaks, potential safety concerns, and system downtime.
One way to prevent these issues is to build your fluid systems with tube fittings from a single manufacturer. Claims that tube fitting components can be intermixed and interchanged with those of different manufacturers should be questioned — intermixing and interchanging can be risky and may compromise worker safety. And no one wants to introduce unnecessary risk into their system’s operation.
Fluid system advice — onsite or remote
No worries! Our field advisors are ready to help. Both on-site and remote support is available.
Requesting an evaluation and consultation from a Swagelok Netherlands Field Advisor is an excellent way to start any gas & liquid systems project. We listen to understand your priorities, gather information about your systems and routines, conduct on-site inspections as needed and offer detailed recommendations. Our goal is to identify opportunities to increase reliability while lowering your operational costs and minimizing risk.
Frequently asked questions
The pressure rating of a Swagelok tube fitting depends on the lowest rated component in the system in which it is installed. Sometimes the lowest pressure rated component is a pipe thread, a pressure gauge, or a valve. Other times it will be the pressure rating of the tubing itself, and that will vary depending on the tubing's size, wall thickness and material of construction.
To learn more, download the literature provided at the top of this Web page.
Swagelok tube fittings come completely assembled, finger-tight, and ready for immediate use.
- Fully insert the tube into the fitting and against the shoulder, and rotate the nut to make sure it is finger tight.
- Mark the nut at the 6 o'clock position.
- While holding the fitting body steady, tighten the nut one and one-quarter turns to the 9 o'clock position, and the job is done.
You will need two open-end wrenches (or one open-end wrench and a vise), a Swagelok gap inspection gauge, a tube-cutter or hacksaw, a file (Swagelok deburring tool), and a marker.
NOTE: Above on this web page is a video demonstrating the correct way to install Swagelok fittings from 1/4 inch to 1 inch.
Tapered pipe threads are one of the most common end connections found in industry. They are relatively simple to make up, however they always need a sealant since there are designed-in gaps between the male and female threads.
PTFE tape fills in the gaps between crests and roots to prevent system fluids from penetrating connections, providing reliable sealing in applications up to 450°F (or 232°C). To complete this task, you will need an open-end wrench, a dry soft-bristled brush, and a roll of PTFE tape (a vise is optional).
NOTE: Above on this web page is a video on preparation, tape size, wrapping procedures, and subsequent tightening.
Do not mix or interchange product components with those of other manufacturers. Doing so voids the Swagelok warranty.
Generally it's best to use like materials. There are exceptions.
Example: if you have stainless steel tubing, use stainless steel ferrules and fittings. On plastic tubing, use plastic ferrules and fittings. The reason for matching materials is simple: You want the ferrules to be stronger than the tubing so that the ferrules can swage onto the tubing and lock into place.
If the ferrules are made of softer material than the tubing, you won't get that swaging action. Brass, for instance, is softer than stainless steel. So brass ferrules won't give you the full swaging action on stainless steel tubing.
NOTE: Please see the video above on this page about selecting proper materials when building a fluid system.
One advantage of the two-ferrule fitting design is the ability to reuse the body without leaks. Most of the cost of replacement is in the fittings, not the nuts and ferrules. Sometimes you don't even have to replace the ferrules.
Before disassembly, mark a line along the nut and body flat and use these marks to ensure that the fitting is reinstalled properly.
NOTE: Above on this web page is a video demonstration of the procedure.
If you have made changes in the system design, by moving a fitting to a new location or changing the tubing, you can't re-use the nuts and ferrules, but you can still re-use the fitting bodies.
For personalized, up-to-the-minute answers to sales and support questions, please use green buttons on this page to request details/quote.
If you prefer to find answers yourself, visit products.swagelok.com, register for an account, and start exploring. Anyone can register, and completing the entire registration form will allow you to view pricing, order online, request quotes, store favorite products, assign customized part numbers, and save or forward your shopping cart.