PFAS Quick Reference Guide
Swagelok Products PFAS Quick Reference Guide
Selecting the right products and ensuring compliance with regulations are crucial for maintaining safety, performance, and legal adherence in various industries. Swagelok's offers extensive expertise to assist customers with any questions regarding PFAS in Swagelok products. Customers can reach out for product selection assistance to make informed decisions and for any PFAS documentation requirements. Learn about fluorochemicals, including what they are, how they’re used in Swagelok products, and important safety and regulatory details.
Facts About Fluorochemicals
PFAS
Per- and Polyfluoroalkyl Substances include nearly every substance containing fluorine Per- and Polyfluoroalkyl Substances are a group of over 10,000 fluorinated substances including stable fluoropolymers such as FKM, FFKM and PTFE which are used as critical seat and seal materials in many Swagelok products. There is only one definition for PFAS, Per- and Polyfluoroalkyl Substances, which includes nearly every substance containing fluorine.
Fluorine has the highest electronegativity of any atom meaning that it forms the strongest possible bonds in organic molecules (molecules having a carbon backbone). Polymers containing fluorine such as PTFE, FFKM and FKM have extreme chemical and temperature resistance. Due to the unique properties of fluorine, fluoropolymers are irreplaceable (without reducing performance).
Research indicates that not all fluorochemicals should be regarded as the same. Not all fluorochemicals have been proven to be hazardous to health nor do they all bioaccumulate. Fluoropolymers, specifically, have been proven to be of low concern (PLC). Some short chain fluorochemicals (primarily C8) have been linked to health hazards and/or bioaccumulation. Major fluoropolymer manufacturers have voluntarily committed to reduce non-polymeric PFAS emissions (2024: 0.009% to air; 0.001% to water; 2030: 0.003% to air; 0.0006% to water*)
Technical communities such as Performance Fluoropolymer Partnership (PFP) and Fluoropolymer Products Group (FPG) both advocate for a balanced, science-based approach to regulations that consider essential and non-essential uses to prevent the unintended consequences that the complete ban of all fluorinated substances would have on sectors that rely on them for critical use. *Manufacturing-Programme-Press-Statement-26-March-2025-.pdf
Optional Seat and Seal Materials in Swagelok Products
Many Swagelok products have seat and seal options for fluid systems that do not require the elevated chemical and temperature resistance that fluorinated seat and seal materials provide. Due to the absence of fluorine in these seat and seal options, product temperature ratings with these options are typically lower than the standard rating.
Seat and seal materials that are PFAS-free
- PEEK
- Polyimide (i.e. Vespel®)
- UHMWPE
- Alloy X-750
- Nitrile (i.e. Buna-N, Buna-C)
- Ethylene Propylene Rubber
- Polychloroprene (i.e. Neoprene)
Seat and seal materials that contain PFAS
- PTFE
- PFA
- PCTFE
- FKM (i.e. Viton)
- FFKM (i.e. Kalrez®, Simriz®, Perlast®, Chemraz®)
Examples of PFAS Free Product Options:
Swagelok 60 Series Ball Valve

- Alloy X-750
- PEEK
- UHMWPE
- Nitrile (i.e. Buna-N, Buna-C)
- Ethylene Propylene Rubber
- Polychloroprene (i.e. Neoprene)
- Note: stem gland is PTFE coated
Swagelok C Series Check Valve
- Nitrile (i.e. Buna-N, Buna-C)
- Ethylene Propylene Rubber
- Polychloroprene (i.e. Neoprene)
- Note: the inlet gasket is PTFE coated on valves requiring an inlet gasket
Fluorochemical Regulations
Most countries have their own legal system and laws for governing chemical restrictions including the 27 member countries of the European Union (EU). Exceptions are expected for essential uses. The Stockholm Convention is an international treaty that aims to limit persistent organic pollutants; it is an agreement rather than a law.
Chemicals are regulated in drinking water in many countries. Perfluorooctanoic acid (PFOA) is no longer used as a processing aid for fluoropolymers in the United States. Hexafluoropropylene oxide dimer acid (HFPO-DA) is used as a processing aid but does not become part of the polymer. Perfluorooctanesulfonic acid (PFOS) is commonly used in textiles and firefighting foam but is being phased out.