The journey of hydrogen 2 — From design to maintenance: how to build a reliable hydrogen system

Knowledge Base
The journey of hydrogen: from design to reliable maintenance
11:29

Those who after reading Part 1 thought, "We understand hydrogen now," will discover in this second part that the real work only begins then. Because once strategy, expectations and positioning are clear, it comes down to the question: how do you build a hydrogen system that runs safely, stably and efficiently for years?

Hydrogen small2-1We continue our conversation with the same field engineer - someone who not only speaks from theory, but has the experience of real-life installations. Where Part 1 took us into strategic reality, Part 2 explains how you go from design to implementation, where systems become vulnerable, and why the smallest choices end up having the biggest impact.

 

1. Material selection: why hydrogen won't forgive a mistake

The conversation begins where many hydrogen projects end: with materials. Or rather, with the wrong material - because that's what the engineer sees all too often.

Question: How does one determine which materials are suitable for a hydrogen system?
Answer:
"Below 30 bar, we can choose very widely thanks to custom alloys from our catalog. There, brittleness is almost no longer a problem. But above 30 bar, everything changes. Then temperature, pressure and cycle behavior become decisive. Especially elastomers are sensitive: hydrogen diffuses through them faster than through metal. That makes them the weakest link in many systems."

With that, he immediately sets the tone. It's not a question of which material works, but which material works for years, at this pressure and with this temperature variation. That nuance difference determines whether a system works well for the first three months or offers years of reliability.

He explains that hydrogen penetrates many rubbers even when initial tests show no problems. This creeping behavior creates risks that only become apparent when systems are in operation.

"It's not the components that fail. It's wrong choices that slowly come to light."

Swagelok Field Engineer

Read more about materials in our material selection guide

 

That makes one thing clear: material choice in hydrogen is not an afterthought, but foundation.

2. Joints and fittings: where everything stands or falls

Whereas in other gas systems "a leak" is often seen as an easy-to-fix shortcoming, in hydrogen this is a misconception that can lead to downtime, inefficiency or dangerous situations.

Question: Why are connections and fittings so critical with hydrogen?
Answer:
"The smallest molecule seeks the smallest leak path. That means the design should have as few connections as possible. And the connections you do have must be of the highest quality. Thread and hydrogen are not a good combination - Tube Fittings are. These are reproducible, predictable and better rule out the human factor causing problems."

He explains how he regularly encounters systems built with threads from good intentions because that works fine within natural gas or nitrogen. With hydrogen, that doesn't work. Minimal mounting variation that is not a problem with other gases can already lead to measurable leakage with hydrogen.

He sums it up succinctly:

"In hydrogen systems, you have no margin for assembly. It has to be right - or it doesn't work."

Many organizations that switch to Tube Fittings quickly find that their systems become more stable, require less maintenance and have fewer leaks.

It's a change in mindset: no longer how do we make it fit, but how do we eliminate every possible leak path.

 

3. Why pressure regulators are the Achilles' heel of many systems

Question: What makes pressure regulators so vulnerable in hydrogen?
Answer:
"They are incredibly sensitive to contamination. Just one damage of a few microns on the seat - so small you can't see it with the naked eye - can cause significant leakage. And that happens especially during startup, when small particles can still be present in the system."

He explains how these damages occur: during filling, from microparticles that have passed filters, from piping that has not been optimally cleaned, or from burrs that occur during assembly.

The result can be that the pressure regulators no longer close exactly or the system exhibits unpredictable behavior, resulting in operators "looking" for a fault they can't find.

Regulator problems often feel like "the system is reacting strangely," when in reality it is one tiny particle that has not been filtered out in time.

That's why he stresses on three principles:

    • Always place a filter before the regulator
    • Always include seal replacement kit when commissioning
    • Always work cleanly
"With hydrogen, a dust particle is not small - it is destructive."

Swagelok Field Engineer

 

4. The person behind the system: discipline, cleanliness and 4-eye control

In Part 1, he already indicated that humans are the biggest risk. Part 2 makes even more clear why.

This is because during installation, the phase in which the design becomes reality occurs. And that is precisely the moment when small errors can arise that later have major consequences.

Question: Where do most problems arise during installation?
Answer:
"In the little things: connections that are not fully tightened, a fitting that is 'just not' right, tape that slips through in the pipe. Contamination is often underestimated. Man is the biggest variable - and the only one you can't standardize."

He says he has seen installations where the technical components were perfect, but where human inaccuracy led to leaks, inefficiency or rework. This indicates the importance of discipline in this work.

"Hydrogen doesn't require more knowledge - it requires more attention,"

As an example, he cites that making a small mistake can be an issue for installers working in cold conditions, or under time pressure, or in noisy environments.
And he therefore advocates the 4-eye principle: one installer assembles, a second checks. Not because there is no trust otherwise, but because hydrogen needs that level of precision.

 

5. Commissioning: the most exciting moment of any system

After installation comes commissioning: the phase when the system first really comes to life and is put into service. According to the engineer, this is the phase where you can win - or lose - everything.

Question: What makes commissioning so critical?
Answer: "Everything is new: materials expand, pressure stabilizes and filters work." But also: it's the time when contamination still in the pipeline can move to critical components. The startup phase is the most vulnerable phase of a system."

A commissioning process done incorrectly, he says, can lead to the following problems, each with substantial consequences for the system and operations. Consider, for example, damaged controllers. This can necessitate costly repairs and often causes unplanned system downtime, causing production or operational delays. Or incorrect pressure settings increase the risk of unsafe situations, such as leaks or explosions, and can seriously affect system reliability. If there is unpredictable flow, it gives unstable or unexpected flow and can disrupt processes, resulting in variations in product quality or damage to sensitive components. You may encounter leaks that seem untraceable. These leaks are difficult to detect, making maintenance more complex, costly and potentially dangerous. And finally, false indications in detection systems may occur. Unreliable sensor information can result in problems not being detected in a timely manner, with all the implications for safety and efficiency.

So what are the solutions to these challenges?
For a successful commissioning process, it is essential toslowly pressurize the system. Pressurizing the system gradually prevents damage and gives room to detect anomalies. Always keep measuring and continuously monitoring parameters ensures that any problems are noticed immediately. Be sure to take your time. Working carefully and without time pressure is conducive to system quality. Keep investigating every anomaly. Deviations should not be ignored, but thoroughly analyzed. And finally, the advice is never to "just push through" something when something is wrong. Continuing despite errors can lead to bigger problems; stopping and correcting is always necessary.

 

6. Detection and monitoring: not a luxury, but foundation

In a gas like nitrogen, you can work relatively safely with limited monitoring. In hydrogen, this is irresponsible.

Question: What detection methods do you think are indispensable?
Answer:
"Helium leak detection and formation gas are the gold standard. But besides that, I recommend everyone to buy a hydrogen sniffer. Those things don't cost much and they give you instant insight. You can't build on 'we think it's good.' You have to measure." He also emphasizes that no hydrogen system is 100 percent tight. That's not a bad thing - as long as you have a grip on the leak rate and know where limits are. Monitoring is thus not only a safety measure, but also a way to understand performance and plan maintenance.

 

7. Scaling up: why larger systems have different risks

Scaling up is often seen as a "bigger version of the same system."
In reality, it is a completely new discipline.

Question: What risks only arise when scaling up?
Answer:
"Discipline does not automatically scale. You build a pilot with three people who can explain everything to each other. A complete plant you build with hundreds of people. Then consistency becomes the biggest risk." It can be imagined that the larger the plant, the greater the number of connections with a chance of variation in assembly, the greater the dependence on procedures and the impact of one small mistake.

It is the phase when project management, documentation and training suddenly become more decisive than technology.

 

8. The future of hydrogen: modularity & infrastructure

Part 1 already indicated that hydrogen is not hype but a realistic building block in Part 2 it becomes clear where the real acceleration is going to occur.

In the future we can think of that offshore wind farms produce hydrogen directly and existing gas pipelines are used for transportation. Energy storage is going to be decentralized and modular and fuel cells will start to drop n cost. We can assume that electrolyzers will become much more efficient. Also, industry clusters will be connected through the "hydrogen backbone."

The Swagelok engineer emphasizes that modularity will make the difference:

"We are moving away from one big plant. The future consists of many small, flexible units that you can scale up and down."

This vision makes hydrogen not only technically feasible, but also economically attractive.

 

 

In conclusion: what we learn from Part 2

Part 2 shows that hydrogen is not a business of big statements, but of small details.
The quality of a system is determined by many different components such as: choice of materials, fittings, cleanliness, pressure regulators and detection. This combined with commissioning, maintenance plan and discipline on all fronts. And - more than anything - by attention. Because the smallest molecule in the world compels us to the greatest craftsmanship.

Background hydrogen