The journey of hydrogen 1 — Why hydrogen is more difficult than it seems

Knowledge Base
The journey of hydrogen - Why hydrogen is harder than it looks part 1
6:08

In many discussions, hydrogen seems the ideal energy carrier: clean, flexible, applicable in industry and mobility, and ideally suited for storing renewable energy. But those who really step into the world of hydrogen discover a reality that is more complex and technical than many people expect. Behind the press releases, pilot projects and ambitious goals lies a daily practice in which design choices, materials, flow dynamics and human behavior make the difference between a robust system or a risky one.

Hydrogen small2For this knowledge base article, we interviewed a field engineer who has been designing, testing and optimizing hydrogen systems for more than a decade. His insights are honest, sometimes critical, but mostly valuable to anyone involved in hydrogen projects.

 

First steps: curiosity, wonder and a new learning curve

 Question: How did you get into the hydrogen world?
Answer:
"It actually started quite innocently. I had been working within gas and liquid systems for years and saw hydrogen popping up more and more often in customer requests. And one day I thought: there's something going on here. The technology, the safety, the innovation - this is exactly the kind of puzzle that makes me happy. From that moment on, I started to fully immerse myself in it." That step turned out to be the start of a long learning curve. A learning curve he says awaits every engineer once you start treating hydrogen seriously.

Question: What was the biggest learning curve in the beginning?
Answer:
"That hydrogen is really completely different from natural gas or nitrogen. Everything you're used to - flow, volume calculations, material selection, seals - works just a little differently. Even thermodynamic effects behave differently. You soon realize: I have to rethink my whole way of thinking."

"Hydrogen forces you to learn to look again."

Swagelok Field Engineer

Where misunderstandings arise: the gap between policy and technology

Anyone who follows the energy transition regularly hears statements like, "We are going to deploy hydrogen on a large scale," or "The hydrogen economy is coming." But according to our expert, the reality is different.

Question: What do you think is the real role of hydrogen in the energy transition?
Answer:
"Hydrogen is becoming crucial, but not everywhere. It is indispensable in heavy industry, because electrification is simply not enough there. And it is the way to store surpluses from solar and wind. But the reality is: you don't replace a hundred-year-old infrastructure in five years. People sometimes forget that."

That nuance is important. Hydrogen is not a silver bullet.
The expert regularly sees political or public expectations rising faster than what technology can deliver.

"Many people think we'll switch over tomorrow. But we are in the middle of an infrastructure transition that has taken decades to build."

Swagelok Field Engineer

TechTalk Hydrogen

TechTalk picture Our ENA half-hour technical presentation. In this video, an expert shares their knowledge on a specific topic, with numerous practical examples, applications, and advice.

More Techtalks

 

Oversizing: the silent cost no one talks about

The conversation reveals that many designers unknowingly make wrong choices precisely because they are copying their experience with natural gas to hydrogen.

Question: What mistakes do you see most often in designs?
Answer:
"Over-dimensioning, without a doubt. Engineers often keep speeds too low because they fear erosion. But with hydrogen, erosion hardly plays a role. As a result, pipes are chosen far too large - and systems too expensive."

He continues:

"We work daily with customers who are shocked when we run through their line-size calculations. It's not that their calculations are bad - it's that they calculate as if they were still in the natural gas world."

Applying larger pipes results in higher costs. In addition, using more material leads to an increase in the number of joints, which increases the risk of leaks. A bulkier system also entails increased maintenance costs.

 

The crucial difference: laminar flow

During the conversation, he repeatedly highlights one engineering design principle that he believes receives too little attention.

Question: Why is laminar flow so important with hydrogen?
Answer:
"Laminar flow ensures stability. Especially in systems where a fuel cell is in the chain. A fuel cell wants a calm, steady flow. Turbulence causes instability, inefficiency and sometimes even error messages. It is one of the most underestimated design rules."

He describes laminar flow as "the quiet power of a good system."
Where turbulent flow chases molecules through the pipeline in chaotic patterns, laminar flow provides energy efficiency and predictable behavior.

And that very predictability is golden in hydrogen systems.

 

The most underestimated risk: humans

Our field engineer is careful to criticize, but clear on one subject:

"Components rarely fail because of poor quality. They fail because of installation errors."

Swagelok Field Engineer

Below are examples of errors found in practice:

    • wrong tightening
    • wrong tape
    • contamination in piping
    • insufficient cleanliness during installation
    • Threaded connections that do not close
    • no four-eye check

We work with the smallest known molecule, but the greatest source of measurement inaccuracy remains the most unpredictable variable in the entire system: humans.

 

Why hydrogen is safer than many people think (if you do it right)

We ask him about the persistent perception that hydrogen would be extremely explosive.

Question: What do you think is the most dangerous misconception?
Answer:
"That hydrogen is inherently dangerous. It isn't. What is dangerous is a poorly designed or poorly maintained system. And poor ventilation inside. Because hydrogen rises. If you understand how it behaves, you can actually build very safe installations."

He emphasizes that ventilation within installations is the key.

 

To conclude part 1: the essence

This knowledge bank session makes one thing clear:
hydrogen is no hype, no simple technology and no obvious solution.
It is a field that requires curiosity, nuance and technical skill.

Where hydrogen will make a difference?

You'll find out in Part 2.

Background hydrogen