Understanding modern gas distribution systems: part 1

Knowledge Base
Optimizing Modern Gas Distribution Systems: Key Insights
7:40

Modern gas distribution systems are becoming increasingly important in environments where safety, reliability and purity are paramount. From laboratories and universities to the chemical industry and high-tech sector, the need for accurate, efficient and future-proof gas supplies is growing everywhere. How do you make the right choices in design, material, layout and safety?

In these Knowledge Bank sessions, we speak with a Swagelok expert. He shares insights from dozens of projects-from central loop lines to high purity systems-and explains which design choices really make the difference. We also discuss common risks, typical errors in existing installations and how organizations can future-proof their systems without immediately rebuilding.

The topics covered in this series of knowledge base articles:
  • Part 1: The role of the market and related applications and how to avoid wasting gas
  • Part 2: System design as the foundation
  • Part 3: What does the operation of a modern gas distribution system depend on? What does preventive maintenance bring and isn't it more expensive?
  • Part 4: The main concerns in the management and maintenance of a gas distribution system and the importance of standards.

 

Market and applications determine the deployment of gas distribution systems by sector

In this session, discover how modern gas distribution systems are becoming increasingly important for sectors as diverse as laboratories, industry and universities. Which markets are growing the fastest, where are the biggest challenges, and how do you make the right choices for safety, efficiency and compliance? Read on and get a fresh perspective on the trends, risks and design trade-offs that will determine a future-proof gas supply.

In what markets are gas distribution systems used most critically?
Gas distribution systems are essential for laboratories, pharmaceutical companies, universities and the chemical industry working with pressurized gases. When small amounts of gas are needed in the workplace, a solid system ensures safety and accuracy.

What differences exist between industries such as chemical, semiconductor, food and education?
Although the principles are similar, the biggest differences are in the purity levels required and the types of gas used. Universities and the semiconductor industry often work with very clean or specialty gases. These gases can quickly become contaminated, which is why the systems must be extra well designed.
The gas mix varies by industry, and each industry has its own risk profile.

Where are uptime requirements most stringent?
In laboratories, the chemical and semiconductor sectors, availability is most important. Downtime there quickly leads to high costs because processes must not be interrupted. In education, things are different: setups change more often and uptime requirements are less stringent.

Which markets are growing the fastest and what does that require of design?
Stricter emissions and energy requirements are increasing demand for modern gas distribution systems across all industries. Organizations want to measure and control processes more accurately, making a reliable and clean gas supply increasingly important. This requires systems that support safety, efficiency and sustainability from the design stage.

How does the decision structure differ by sector?
The differences lie primarily with individual organizations. Facility management and QHSE usually make the most important decisions because gas distribution directly affects safety and management. End users join later in the process, as they will eventually work with the system.

What role do QHSE and compliance play in investments?
This plays a big role. Gas distribution involves safety risks, such as fire and explosion. Therefore, safety and compliance are at the heart of organizations' decisions. Often these tasks are merged with facility management.

When are companies open to new investments?
Security, ease of use and uptime are essential. A cumbersome system increases the likelihood of errors and risks. Organizations also increasingly see cost as a driver; those who take a critical look at gas consumption often discover considerable waste.

"Organizations want to measure and control processes more accurately, making a reliable and clean gas supply increasingly important."
Swagelok-Icon-SVG

Swagelok Netherlands

Sales Engineer

Gas-Lines

By smartly measuring and optimizing, you can prevent waste and structurally reduce the cost of gas usage.

At a time when sustainability and cost optimization are increasingly high on the agenda, efficiently managing gas consumption is crucial for any organization working with gas distribution systems. Wastage often goes unnoticed, but can lead to substantial additional expenses and unnecessary strain on installations. In this section, we dive deeper into the causes of hidden gas losses, how to make waste measurable and what concrete steps will yield immediate savings. We also discuss how smart design choices and cooperation between specialists, facility management and users contribute to structural cost control and the responsible use of scarce gases such as helium.

Where do the biggest hidden gas losses occur within facilities?
The main loss points are:

  1. Connection of bulk gas to the network, where leaks become visible as large ice deposits under cylinders.
  2. Gas distribution boxes that have barely been maintained since construction, with outdated valves causing leaks.
  3. End users modifying pipes or connections themselves without sufficient knowledge, leading to unsafe or leaking situations.

What losses are often underestimated by operations?
Total gas consumption is often underestimated. A cylinder seems cheap, but structurally excessive consumption (for example, 15 additional cylinders per year) leads to significant costs-especially with specialty gases such as helium. End users usually do not see invoices and facility managers do not always have insight into actual consumption. Regular consultation between specialists, facility management and users is essential to get consumption and losses clear.

How do you make waste measurable with data?
By comparing usage points to total gas consumption. If 40 use points have a certain average consumption, but the total is 30% higher, this almost certainly indicates leakage or inefficient use. The key is collaboration between end users and whoever manages gas procurement.

What immediate changes create quickly visible cost savings?
Sealing and optimizing setups directly reduces gas consumption. In addition, the number of failures and downtime decreases because sensors go off less often due to leaks. This reduces costs AND increases productivity.

How do you manage the cost and scarcity of expensive gases such as helium?
By ensuring a well-designed quality distribution system and by taking a critical look at actual gas consumption at points of use. Discipline in standard procedures and proper alignment with plant quality help reduce consumption.

Does distribution design play a role with specialty gases?
Certainly. Systems for helium, for example, that are continuously pressurized require very high installation standards. A more decentralized design with high-quality components can minimize consumption. In addition, gas recovery (for example, after experiments) can be integrated to reuse helium.

 

Read more in Part 2 about the importance of good design and what to look out for to avoid operational challenges in gas distribution systems.

Read part 2 Swagelok Gas distribution systems
gas distribution systems